Skip to main content
Visitor II
May 20, 2024
Question

Request to check the authenticity of M24C04

Hello, I'm Jade.
We are using ST Micro's M24C04 parts.
I bought the parts, but the shape of the imprint is different, so I'm inquiring about which one is real.
Please refer to the picture below. Lot information is the same, but ST mark is different.

Thank you

JadeYoon_0-1716198108597.png

JadeYoon_1-1716198114201.png

 

 

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
May 21, 2024

Welcome @JadeYoon, to the community!

The labelling does indeed look very strange. However, you cannot definitively conclude from this that it is fake device.

If you have a sticker on the packaging with a bulk ID on it, you are welcome to send me a legible photo via PM so that I can check it. However, please do not post it here in the community to avoid abuse.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.