Skip to main content
bsaleh
Associate
Dec 29, 2006 5:09 AM UTC
Question

Replacing IGBT's with MOSFET's on STEVAL-IHM003V1

Posted on December 29, 2006 at 06:09

Replacing IGBT's with MOSFET's on STEVAL-IHM003V1

This topic has been closed for replies.

2 replies

bsaleh
bsalehAuthor
Associate
Dec 3, 2006 7:43 PM UTC
Posted on December 03, 2006 at 20:43

Hello,

Would anybody recommend a type of MOSFET that would be suitable to replace the IGBT's with on STEVAL-IHM003V1 power board? I want to run my power board with an input of 15 volts which cant be do without replacing the IGBT's with MOSFET's.

Thanks in advance

Regards

sisto
Associate II
Dec 29, 2006 5:09 AM UTC
Posted on December 29, 2006 at 06:09

The IGBT is an hybrid device which tipically integrate a bipolar transistor to drive a power ''N'' MOS.

This solution concurs to reduce the input capacitance to obtain an high speed power device.

The value of input capacitance of a power Mos is inversely proportional to RDS_ON; that means high current device == high input capacitance and consequently low speed (and maybe high temperature to dissipate).

So it depends on your application: if You need speed and power You must use IGBT.

In any case You must see the board STEVAL schematic for actual IGBT command logic and evaluate the compatibility for a direct gate MOS command.

Sixtus

:)