Skip to main content
daniel8
Associate III
Dec 10, 2009 5:36 PM UTC
Question

Remapping interrupts

Posted on December 10, 2009 at 18:36

Remapping interrupts

This topic has been closed for replies.

2 replies

tomas23
Visitor II
May 17, 2011 7:59 AM UTC
Posted on May 17, 2011 at 09:59

You have to dig into assembly :)

Check attached files, beware of start-up codes and changes in linker files, they are CRITICAL to proper IVT forward.

Modify according to your needs.

daniel8
daniel8Author
Associate III
May 17, 2011 7:59 AM UTC
Posted on May 17, 2011 at 09:59

I am trying to implement the fix for Rev. G silicon where I do not remap the FMI to jump to Bank0 , and instead just jump to 0x80000 to execute the code. The problem is the interrupts do not remap, and I cannot figure out how remap them. If I set in Bank1 the irq_handler address to bank 0, the interrupts work, but then of course the interrupts do not work in bank1 (which is a problem).

I would have thought it would have remapped itself once the new code initialized, but that is not the case. Any suggestions would be appreciated. THanks