Skip to main content
babidesai123
Associate III
May 8, 2003 3:19 AM UTC
Question

regarding secondary flash as code space

Posted on May 08, 2003 at 05:19

regarding secondary flash as code space

This topic has been closed for replies.

3 replies

babidesai123
Associate III
May 17, 2011 9:53 AM UTC
Posted on May 17, 2011 at 11:53

Hello,

Can anyone tell me,for general IAP design why it is recomended that

secondary flash should contain the IAP code & primary as main application code??

Apart from the large memory area what is the major difference between the two.

If assume that application cdoe is small enough to fit into the 1 sector of secondary flash , then it is advisible to use secondary as application code area & primary as IAP code or no....

PLZ clarify
babidesai123
Associate III
May 17, 2011 9:53 AM UTC
Posted on May 17, 2011 at 11:53

Thanks alot..

purvi

joseph2399
Associate II
May 17, 2011 9:53 AM UTC
Posted on May 17, 2011 at 11:53

Secondary Flash has higher priority than the Primary Flash (see Figure 51, data sheet), other than that, they should be the same. If the VM register is setup properly, IAP can reside in the Main Flash at power up also.