Skip to main content
wileti
Associate II
Sep 11, 2007 4:02 AM UTC
Question

redeclared error

Posted on September 11, 2007 at 06:02

redeclared error

This topic has been closed for replies.

2 replies

wileti
wiletiAuthor
Associate II
Sep 10, 2007 3:02 PM UTC
Posted on September 10, 2007 at 17:02

Hi all,

I´m using ST72F63B microcontroller and after compilation the below messages are prompted:

#error cpst7 io72263.h:7(14+4) redeclared localized PADR

#error cpst7 io72263.h:9(14+5) redeclared localized PADDR

#error cpst7 io72263.h:11(14+4) redeclared localized PBDR

#error cpst7 io72263.h:13(14+5) redeclared localized PBDDR

and so on...

In actual fact, I´ve declared these variables once a time in io72263.h file as described below:

volatile char PADR @0x00; /* Port A Data Register */

volatile char PADDR @0x01; /* Port A Data Direction */

volatile char PBDR @0x02; /* Port B Data Register */

volatile char PBDDR @0x03; /* Port B Data Direction */

volatile char PCDR @0x04; /* Port C Data Register */

volatile char PCDDR @0x05; /* Port C Data Direction */

volatile char PDDR @0x06; /* Port D Data Register */

volatile char PDDDR @0x07; /* Port D Data Direction */

and so on...

Thus, I have no idea for these error messages. Where should I try harder in order to find out the problem?

Thank you for any help,

Wilson

luca239955_st
Associate II
Sep 11, 2007 4:02 AM UTC
Posted on September 11, 2007 at 06:02

the message is quite clear: you declared every var more than once.

Maybe you include the same file twice, or you include a file with the declarations in a file where the vars are already declared: it should be easy to find out.