Skip to main content
babidesai123
Associate III
Jan 9, 2004 1:52 PM UTC
Question

reading the falsh content using JTAG

Posted on January 09, 2004 at 14:52

reading the falsh content using JTAG

This topic has been closed for replies.

7 replies

babidesai123
Associate III
May 17, 2011 9:53 AM UTC
Posted on May 17, 2011 at 11:53

Hi,

Can we read the flash memory (full or sector) using the JTAG programming??provided that flash sector is not protected.

if yes the what are the steps??

Can u give detail steps to read the flash mem content using JTAG?

[ This message was edited by: Purvi on 11-04-2003 08:54 ]
sjo
Associate III
May 17, 2011 9:53 AM UTC
Posted on May 17, 2011 at 11:53

If using the Flashlink do an upload in the JTAG/ISP section

Regards

sjo
babidesai123
Associate III
May 17, 2011 9:53 AM UTC
Posted on May 17, 2011 at 11:53

just now i tried with that ..but it's showing the dialog box showing

''device upsd3234A is currently not supported under psd pro''

plz help
yu-jun
Associate
May 17, 2011 9:53 AM UTC
Posted on May 17, 2011 at 11:53

In the PSDsoft Express there si a fuction: STMicroelectronics Conventional Programmers.

Run it, you should come into a dialog.

In the dialog you press the button --- Upload. the data in the uPSD can been load.

If the data is protected, you can't do it.
sbencke3
Associate III
May 17, 2011 9:53 AM UTC
Posted on May 17, 2011 at 11:53

I am trying to do the same thing, and I receive the same response. Did you resolve this problem ?

jdaniel
Associate III
May 17, 2011 9:53 AM UTC
Posted on May 17, 2011 at 11:53

Yes, you can... in the ''Step 2'' section, the first box normal has ''Program/Verify'' selected or something of the like. Just change it to upload.

sbencke3
Associate III
May 17, 2011 9:53 AM UTC
Posted on May 17, 2011 at 11:53

Ok, but in this section I can't read the device, can I?