Skip to main content
fa_it
Associate III
Nov 9, 2005 6:02 AM UTC
Question

RAM debug macro files for JLINK and IAR compiler

Posted on November 09, 2005 at 07:02

RAM debug macro files for JLINK and IAR compiler

This topic has been closed for replies.

3 replies

fa_it
fa_itAuthor
Associate III
Nov 1, 2005 6:03 AM UTC
Posted on November 01, 2005 at 07:03

Does any one have a macro file, to enable RAM debug when using JLINK and IAR compiler?

Or is there another way to get RAM debug to work in IAR.

Best regards,

Frank Andersen

fa_it
fa_itAuthor
Associate III
Nov 1, 2005 8:40 AM UTC
Posted on November 01, 2005 at 09:40

I have the IAR ver 4.30A, and a JLINK kicstart and kit with the STR711 from IAR. The problem is that all the examples are programmed into flash, if I select the configuration file to the Linker to xxxxx_ram.xcl, then the code is not excuted from RAM.

For the Atmel SAM7 there is a macro for Debugger, to be used when debuging in RAM, that is file I am looking for to the STR71x

Best Regards,

Frank Andersen

e239955_stm1_stmicro_com
Associate III
Nov 7, 2005 8:54 AM UTC
Posted on November 07, 2005 at 09:54

Hi,

I'm using winIDEA with IAR, but I think you should uncheck the flash loader box,

Manu

________________

Attachments :

iar.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtOo&d=%2Fa%2F0X0000000aPT%2F7YLgQQsWEgqWPSY0t7LWT0iLhemmHIeLIQvBl90D_f0&asPdf=false