Skip to main content
abogani9
Associate II
Jun 16, 2009 6:33 AM UTC
Question

Raisonance CodeCompressor through STVD 4.1.2

Posted on June 16, 2009 at 08:33

Raisonance CodeCompressor through STVD 4.1.2

    This topic has been closed for replies.

    2 replies

    mozra27
    Visitor II
    May 17, 2011 1:03 PM UTC
    Posted on May 17, 2011 at 15:03

    Hi Bogani,

    The code compressor with STVD use the defined option: -AOF -NOHEX -C -T(2) if you have an issue with this configuration you can check an other specific option by running the command line:

    The command line syntax is:

    \Bin\ccompst7_7.exe aofname [options]

    Where options may be:

    -C complete process (in lining, factorizing, saving)

    -I inlining process without any limitation

    -IN(value) inlining process with number of in lined functions limited up to value

    -F factorizing process without any limitation

    -FN(value) factorizing process with a number of factorizations limited up to value

    -FS(value) factorizing process with a minimum gain of value bytes per factorization

    -FD(value) factorizing process with a maximum gain of value bytes per factorization

    -LF log file generation

    -T(variant) Define the processor variant: 0 for ST7 (default) and 2 for STM8.

    -V(level) verbose level on level value

    -[NO]AOF generate [not] an OMF-ST7 file (default is NOAOF)

    -[NO]HEX generate [not] a HEX file (default is HEX)

    -[NO]BIN generate [not] a BINARY file (default is NOBIN)

    Regards

    mozra

    abogani9
    abogani9Author
    Associate II
    May 17, 2011 1:03 PM UTC
    Posted on May 17, 2011 at 15:03

    Hi,

    I have noticed that the just released STVD 4.1.2 support the Raisonance's codecompressor. I found this feature very useful so I go immediatly to test it.

    Unfortunately it hang without end on my personal computer at:

    [...]

    LINK/LOCATE RUN COMPLETE, NO ERROR FOUND.

    ccompst7_7.exe Debug\program.aof -O(Debug\program.aof) -AOF -NOHEX -C -T(2)

    [...]

    It is also eat the 50% of my AthlonX2 5600+ (2,9Ghz).

    Could anyone point me at workaround?

    Thanks!

    Ciao,

    Alessio