Skip to main content
master
Associate
Apr 19, 2011 8:42 AM UTC
Question

radiation from mobile phones -> auto reset?

Posted on April 19, 2011 at 10:42

Hello,

I have just finished my project, but unfortunately I have a problem at the end. ;) My Stm8s Discovery is in a plastic box together with a cell phone. When the cell phone get switched on, the

microcontroller

resets itself. Is this normal? Has anybody of you a glue to solve this problem? Maybe without extra shielding? When I put the mobile more than 15cm away from the

microcontroller

, it works... but the box is small...

Thanks in advance

Klaus

#shielding-cell-phone-reset
    This topic has been closed for replies.

    1 reply

    brazov22
    Associate III
    Apr 19, 2011 1:46 PM UTC
    Posted on April 19, 2011 at 15:46

    put the discovery board inside a aluminium paper :)