Skip to main content
icwang
Associate II
Apr 18, 2006 3:54 AM UTC
Question

Question : RLink used in STVD7

Posted on April 18, 2006 at 05:54

Question : RLink used in STVD7

This topic has been closed for replies.

6 replies

icwang
icwangAuthor
Associate II
Apr 12, 2006 4:02 AM UTC
Posted on April 12, 2006 at 06:02

Are aLL ST7 spported in STVD7 use RLink tool to debug and Programmer?

Currently I use st7flite series. I want to develop ST MCU in STVD7 use RLink.

Pls kindly give some advice.

Thanks.

luter
Associate III
Apr 12, 2006 5:46 AM UTC
Posted on April 12, 2006 at 07:46

Hi.

Go in project settings->MCU selection and choose device u need. if green light near Icd RLink shines this device is supported by RLink.

icwang
icwangAuthor
Associate II
Apr 12, 2006 6:33 AM UTC
Posted on April 12, 2006 at 08:33

Thanks

I do so. but i still connect to mcu.

PLS help me.

luter
Associate III
Apr 12, 2006 6:47 AM UTC
Posted on April 12, 2006 at 08:47

I do not understand your question.

Did u intall driver for RLink?

icwang
icwangAuthor
Associate II
Apr 15, 2006 12:48 AM UTC
Posted on April 15, 2006 at 02:48

I have install the driver for RLink in my computer.

I use st7flit15b, my configration is :

ICC CONNECTOR MCU

GND(1,3,5,10) ----> ST7FLIT15B(1)

VDD_APPLI(7) ----> ST7FLIT15B(2)

ICCDATA(2) ----> ST7FLIT15B(12)

ICCCLK(4) ----> ST7FLIT15B(11)

ICCRESET(6) ----> ST7FLIT15B(3)

ICCSEL/VPP(8)

ICCOSC(9)

I use this congfigration in STVD7 and RIDE ,both can't to connect to MCU.

I still connect to the mcu, pls help me.

luter
Associate III
Apr 18, 2006 3:54 AM UTC
Posted on April 18, 2006 at 05:54

Well, it looks like the problem is your application board. Are u sure that all connections are rights, mcu is properly installed on application board?