Skip to main content
MNage
Associate II
June 4, 2020
Question

Question regarding the Programmer(Jtag) for ST10F276E supported

Hi Team,

I am working with ST10F276E Micro controller being MDK-arm not supported installed C166 toolchain eveluation version and it was successfully build.

My question that i want to download the code into flash (microchip IC) i found something like 

JTAGjet-166(http://www.keil.com/dd/chip/3545.htm)its with IAR embedded workbench.

So, is there any flash utility to support downloading the hex file into the flash using UART calble or any ST-link/u-link debugger(JTAG) to purchase..???

Kindly suggest.. :)

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
June 4, 2020

Like ST10 Flasher?​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MNage
MNageAuthor
Associate II
June 4, 2020

hope u got my question i mean to say do i no need to use any STlink debugger (adapter) as interface to pc and board (if need to use i dont have connection setup at boradside) so directly thrpugh UART interface can ST10 flasher will work...????

Tesla DeLorean
Guru
June 4, 2020

You're using an obsolete device. What active support there used to be has moved on.

I'm answering the question : "So, is there any flash utility to support downloading the hex file into the flash using UART cable"

Yes, there's a tool called ST10 Flasher that does exactly that.

https://www.st.com/resource/en/application_note/cd00052666-programming-the-st10f27x-embedded-flash-using-the-st10flasher-tool-stmicroelectronics.pdf

Not sure how well it handles COM ports with high indicies, really OLD software.

https://community.st.com/s/question/0D53W000004lNH9SAM/how-can-i-get-the-st10-flasher-tool

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..