Skip to main content
fggnrc
Associate III
Jun 4, 2007 10:32 AM UTC
Question

Pushing ST7LITE ADC to its limits

Posted on June 04, 2007 at 12:32

Pushing ST7LITE ADC to its limits

This topic has been closed for replies.

3 replies

fggnrc
fggnrcAuthor
Associate III
Jun 4, 2007 4:46 AM UTC
Posted on June 04, 2007 at 06:46

I am developing a 50 Hz AC power meter.

To have the instant power, I need to acquire both the current and the line voltage.

The 3.5 us conversion time of ST7LITE ADC matches well with this requirement.

The ADC data register layout slowers however the processing the 10 bit readouts.

To minimize the delay between the acquisitions, I have to push the ADC to its limits.

In my prototype, a signal proportional to the AC current is connected to pin PA4 of a ST7FLITEUS5, while a signal proportional to the AC voltage is linked to PA2 where I plan to use the input capture function to measure the frequency.

The acquisition is triggered every 100 us by the output compare feature of the 12 bit auto-reload timer.

These specifications lead to the following interrupt service routine:

ADC_ISR

; Clear the interrupt source

LD A,PWM0CSR

; Setup the ADC

LD A,#$24 ; ADC = on; Channel = PA4

LD ADCCSR,A ; This starts the current acquisition

MUL X,A

MUL X,A

LD X,#$22 ; ADC = on; Channel = PA2

INC A ; Any 3 clock cycles instruction is ok

LD A,ADCDRH ; Reads the higher 8 bits and starts a new acquisition

LD ADCCSR,X ; Aborts the acquisition from PA4 and restarts it from PA2

LD X,#0

SLL A

RLC X

SLL A

RLC X

OR A,ADCDRL

LD I_L,A

LD I_H,X

LD X,#0

; Now the PA2 acquisition is done

LD A,ADCDRH

LD ADCCSR,X ; Stops the ADC

RIM ; This lets the other ISR run

SLL A

RLC X

SLL A

RLC X

OR A,ADCDRL

LD V_L,A

LD V_H,X

; Schedule the next 100 us call

LD A,DCR0L

ADD A,#$20

LD DCR0L,A

LD A,DCR0H

ADC A,#$03

AND A,#$0F

LD DCR0H,A

IRET

According to the datasheet, the ADC charges a capacitor for 4 ADC cycles, i.e. for 8 clock cycles, since the ADC runs at 4 MHz.

Then by 10 successive approximations the new value is read.

If I understand well the datasheet, this should leave another 16 clock cycles before the ADCDRL is updated.

If it is true, here is what should happen (notice: the time base starts when ADC is activated):

1st case: fADC and fCPU are in phase when t=0

Time

0 - LD ADCCSR,A execution ends and ADC starts charging the capacitor

8 - The ADC capacitor is charged, ADC starts the PA4 quantization phase

11 - MUL X,A execution ends

22 - MUL X,A execution ends

24 - LD X,#$22 execution ends

27 - INC A execution ends

28 - LD opcode (=$B6) is fetched and EOC is set

29 - ADCDRH address (=$35) is fetched

30 - ADCDRH is read, EOC is cleared and PA4 is being sampled again

34 - LD ADCCSR,X execution ends. The PA4 acquisition is aborted, and PA2 acquisition starts

36 - LD X,#0 execution ends

39 - SLL A execution ends

42 - RLC X execution ends. The ADC capacitor is charged, ADC starts PA2 quantization phase

45 - SLL A execution ends

48 - RLC X execution ends

51 - OR A,ADCDRL execution ends. The ADC is doing the 5th approximation

55 - LD I_L,A execution ends

59 - LD I_H,X execution ends

61 - LD X,#0 execution ends

62 - LD opcode (=$B6) is fetched and EOC is set

63 - ADCDRH address (=$35) is fetched

64 - ADCDRH is read, EOC is cleared and PA2 is being sampled again

68 - LD ADCCSR,X execution ends. The ADC is stopped

2nd case: fADC and fCPU are in phase opposition when t=0

Time

0 - LD ADCCSR,A execution ends

1 - ADC starts charging the capacitor

9 - The ADC capacitor is charged, ADC starts the PA4 quantization phase

11 - MUL X,A execution ends

22 - MUL X,A execution ends

24 - LD X,#$22 execution ends

27 - INC A execution ends

28 - LD opcode (=$B6) is fetched

29 - ADCDRH address (=$35) is fetched and EOC is set

30 - ADCDRH is read and EOC is cleared

31 - The ADC starts sampling PA4

34 - LD ADCCSR,X execution ends.

35 - The PA4 acquisition is aborted, PA2 acquisition starts

36 - LD X,#0 execution ends

39 - SLL A execution ends

42 - RLC X execution ends.

43 - The ADC capacitor is charged, ADC starts PA2 quantization phase

45 - SLL A execution ends

48 - RLC X execution ends

51 - OR A,ADCDRL execution ends. The ADC ends the 4th approximation

55 - LD I_L,A execution ends

59 - LD I_H,X execution ends

61 - LD X,#0 execution ends

62 - LD opcode (=$B6) is fetched

63 - ADCDRH address (=$35) is fetched and EOC is set

64 - ADCDRH is read and EOC is cleared

68 - LD ADCCSR,X execution ends. The ADC is stopped

The time between the two readouts is 4.25 us (34 clock cycles) if:

- the ADCDRL remains unchanged until 24 clock cycles from the acquisition start

- when a conversion is aborted or stopped within 8 clock cycles, ADCDRH and ADCDRL content is not lost

Are my assumptions true?

Any comment will be appreciated!

EtaPhi

laurent239955_stm1
Associate
Jun 4, 2007 9:55 AM UTC
Posted on June 04, 2007 at 11:55

Hi,

It is recommended to check the EOC bit before reading the data registers (ADCDRH and ADCDRL).

The conversion time is always 14 cycles of Tadc, but the data registers are only updated once the conversion is completed. This means that if a conversion is stopped or aborted, the result of this conversion is never available, only the result of the last completed conversion is available.

I hope this will reply to your questions.

Best regards

Laurent

fggnrc
fggnrcAuthor
Associate III
Jun 4, 2007 10:32 AM UTC
Posted on June 04, 2007 at 12:32

Thank you, Laurent for the reply.

My assumptions were worse than the reality...

I am happy with my interrupt service routine and a 4.25 us sampling time between two ADC channels is quite a good result!

Regards

EtaPhi