Skip to main content
bruno2
Associate
May 26, 2014 6:55 PM UTC
Question

Pull Up pin

Posted on May 26, 2014 at 20:55

Is there some way to turn off a pull up input for some time and later turn it on on a certain frequency? 

The pull up pin drain too much current.
    This topic has been closed for replies.

    3 replies

    abbas
    Associate III
    May 27, 2014 7:15 AM UTC
    Posted on May 27, 2014 at 09:15

    you can use a timer interrupt handler to turn pull up on and off at a certain frequency

    bruno2
    bruno2Author
    Associate
    May 27, 2014 10:55 AM UTC
    Posted on May 27, 2014 at 12:55

    How can i do that? Can you send me an axample?

    abbas
    Associate III
    May 27, 2014 12:10 PM UTC
    Posted on May 27, 2014 at 14:10

    for example, you config one of your timers like this

    void TIM1_Config(void)

    {

      TIM1_DeInit ();

      TIM1_TimeBaseInit (TIM1_PRESCALER, TIM1_COUNTERMODE_UP, TIM1_PERIOD, 0);

      TIM1_ITConfig (TIM1_IT_UPDATE, ENABLE);

      TIM1_ARRPreloadConfig (ENABLE);

      TIM1_Cmd (ENABLE);

    }

    and in interrupt handler you can do like this, flag_pull_up must be defined as a global variable

    INTERRUPT_HANDLER (TIM1_UPD_OVF_TRG_BRK_IRQHandler, 11)

    {

      if (flag_GPIO_pull_up)

      {

        GPIO_Init  ( GPIOx,  GPIO_Pin, GPIO_MODE_IN_FL_NO_IT );

      }

      else 

      {

        GPIO_Init  ( GPIOx,  GPIO_Pin, GPIO_MODE_IN_PU_NO_IT )

        // write your routine

      }

      flag_GPIO_pull_up

    = !

    flag_GPIO_pull_up

    ;

      TIM1_ClearFlag(TIM1_FLAG_UPDATE);

    }