Skip to main content
grzesiek
Associate
Jul 12, 2004 12:32 PM UTC
Question

PSDsoft Express hangs Windows 2000

Posted on July 12, 2004 at 14:32

PSDsoft Express hangs Windows 2000

This topic has been closed for replies.

5 replies

joseph2399
Associate II
May 17, 2011 10:02 AM UTC
Posted on May 17, 2011 at 12:02

The latest version of PSDsoft is 8.10. Please download and use this version.

It can be found at:

http://www.st.com/stonline/products/families/memories/psm/soft_c2.htm

IMPORTANT:

If you have a PC with HyperThreading or dual processors, be sure to see FAQ #109 at the following FAQ page:

http://www.st.com/stonline/products/families/memories/psm/psdfaq.htm

grzesiek
grzesiekAuthor
Associate
May 17, 2011 10:02 AM UTC
Posted on May 17, 2011 at 12:02

Installation of PSDsoft Express v7.90 on Windows 2000 makes that the system

hangs on boot. Before I had no problem under Windows NT4.0.

Now I have to move to Windows 2000 (polish version).

Effect is always the same, regardless of what other software is installed or

what service packs and what patches are installed.

In one of experiments PSDsoft Express was installed just after Windows itself

and the system also hangs.

Did anybody have such experience? And what to do?
mandar
Visitor II
Jul 7, 2011 10:05 AM UTC
Posted on July 07, 2011 at 12:05

Hello uPSD,

We are also struggling with PSDsoft Express version 7 , it simply hangs the PC during Programming PSD4235G2 Chip.

As you had mentioned in your previous reply , We did try to download the Version 8.10 of PSD express . but unfortunetly its not on the Link mentioned below.

So please can you send us the PSDsoft Express 8.10 version via e-mail to

mailto:mandar.bagul@ge.com

This will be of great help.

-Thanks & Regards-

Mandar Bagul.

Tech Lead.

GE Oil & Gas

Hyderabad, India.

91-40-40220187

jafrica
Visitor II
Jul 19, 2011 4:31 PM UTC
Posted on July 19, 2011 at 18:31

Hi, the links that you posted are dead. Could you also send me a copy of PSDSoft express (latest version)?

mailto:jafrica@wms.com

Thanks

theo23
Visitor II
Jul 22, 2011 1:46 PM UTC
Posted on July 22, 2011 at 15:46

Hello uPSD,

We are also developing with PSDsoft Express.

We did try to download the Version 8.10 of PSD express . but unfortunetly its not on the Link mentioned below.

So please can you send us the PSDsoft Express 8.10 version via e-mail to 

mailto:theo.spalinger@karlstorz.com