Skip to main content
sewen
Associate
Oct 20, 2004 2:23 PM UTC
Question

PSD8xx and non-multiplexed micro - Help with lcd interface

Posted on October 20, 2004 at 16:23

PSD8xx and non-multiplexed micro - Help with lcd interface

This topic has been closed for replies.

1 reply

sewen
sewenAuthor
Associate
May 17, 2011 10:03 AM UTC
Posted on May 17, 2011 at 12:03

I am having trouble getting a non-multiplexed micro (68HC11F1) with a PSD853 to interface with a lcd. I can get my code (with basic changes) to work using a multiplexed micro (68HC11D0) with the PSD and the lcd, so I am sure I am just overlooking something simple with the non-multiplexed setup.

I am using the same data lines to connect the micro, PSD, and lcd. I have dropped the timing down to make sure that it was not to fast for the lcd. Using on-board Chip Select from PSD and using the E signal as the logical qualifier in PSDsoft. Using one pin to act as the register select.

Help anyone....please!!!