Skip to main content
biuro4
Associate II
September 10, 2003
Question

programming ST62E20

  • September 10, 2003
  • 2 replies
  • 780 views
Posted on September 10, 2003 at 08:43

programming ST62E20

This topic has been closed for replies.

2 replies

biuro4
biuro4Author
Associate II
September 10, 2003
Posted on September 10, 2003 at 08:31

Hi,

I am currently designing an application with ST62E20, i realy need it to work with 3V power supply, but when i turn on my design, microcontroller sweetches itself into internal clock state, everything is going slower, when i supply it with 5V everything is OK. There are some option bytes but i've no clue how to change them because i don't have this option in my programmer. What can I do?

Thanks Paul
sjo
Associate III
September 10, 2003
Posted on September 10, 2003 at 08:43

Remember as per the datasheet @ 3v the maximum osc frequency is 4MHz

Regards

sjo