Skip to main content
New.Fish
Associate III
November 8, 2021
Solved

Program STM8 flash

Can I use "STM32 ST-Link Utility" or "STM32CubeProgrammer" to program STM8MCU flash?

If using "STVP", can it automatically detect the STM8MCU type? or require to configure "STVP" for the MCU type to be programmed.

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    November 8, 2021

    As can be seen from the name, STM32 ST-Link Utility and STM32CubeProgrammer can only be used for STM32.

    STVP cannot automatically determine the target MCU, so it must always be specified.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    2 replies

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    November 8, 2021

    As can be seen from the name, STM32 ST-Link Utility and STM32CubeProgrammer can only be used for STM32.

    STVP cannot automatically determine the target MCU, so it must always be specified.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Associate III
    March 10, 2025

    Sir,

    STLINK V2 is hardware and stlink utility is older type programe uploader software and stm32cubeprogrammer also same category. i think though i am not sure that it can't programe stm8 series . please provide what is the reason that it cant programe stm8 series MCU. i have brought STlink-V3MODs . can it programe and debug using STdv ide  to stm8s? if not then what to use to programe and debug stm8 MCU.