Skip to main content
iamlyg98
Associate
Jun 30, 2006 5:22 AM UTC
Question

program internal flash

Posted on June 30, 2006 at 07:22

program internal flash

This topic has been closed for replies.

5 replies

iamlyg98
iamlyg98Author
Associate
Jun 27, 2006 2:17 AM UTC
Posted on June 27, 2006 at 04:17

I want to use STR712,but I don't have JTAG adapter,

How can i download my program to STR712's internal flash.

can I use ISP like philips's LPC series?

or STR712 have other simple ways.

iamlyg98
iamlyg98Author
Associate
Jun 27, 2006 9:10 AM UTC
Posted on June 27, 2006 at 11:10

thanks

but I don't known how can I download my application(hex or bin format)

to STR712's internal flash,and my application can run after power up.

I have no other tool such as JTAG adapter or keil's ULINK.

is there bootloader in STR712 burned by ST before STR712 go out from product line?

xakaicheng
Associate II
Jun 28, 2006 5:43 PM UTC
Posted on June 28, 2006 at 19:43

hi Zouh,

May I download code to internal flash with Wiggler JTAG? I am using EWARM V4.11. Or I have to do it with IAP?

btw, what's the usage of FlashSTR71xF.d79 file?

xakaicheng
Associate II
Jun 29, 2006 3:11 PM UTC
Posted on June 29, 2006 at 17:11

hi Zouh,

I tried use ''FlashSTR71xF.d79'' to download code to internal flash several times, but EWARM4.11 terminated with an error.

My XLINK commands are like this:

-DROMSTART=0x40000000

-DROMEND=0x4003FFFF

-DVECSTART=ROMSTART

-DRAMSTART=0x20000000

-DRAMEND=0x2000FFFF

and I did following steps:

1.in Project -> Options -> Linker -> Output -> Check ''Allow C-spy-specific extre output file''

2.in Project -> Options -> Linker -> Extra Output -> Select ''Simple code'' format

3.in Project -> Debugger -> Download -> Check ''Flash download''

4.in Project -> Debugger -> Download -> Check ''Override default flash loader'' and select file ''FlashSTR71xF.d79''

Is there any procedure I missed?

xakaicheng
Associate II
Jun 30, 2006 5:22 AM UTC
Posted on June 30, 2006 at 07:22

hi,

I can not see the ''Flash Loader Configuration'' dialog box in EWARM V4.11, but I did relocate the base address.

Maybe I have to upgrade to EWARM V4.40A?

thanks!