Skip to main content
fd_it
Associate II
Aug 9, 2005 8:40 AM UTC
Question

Problems with ICP programming ST72F264G2

Posted on August 09, 2005 at 10:40

Problems with ICP programming ST72F264G2

This topic has been closed for replies.

3 replies

fd_it
fd_itAuthor
Associate II
Aug 2, 2005 10:55 AM UTC
Posted on August 02, 2005 at 12:55

When trying to program ST72F264G2 using ST7 STICK, following error occurs:

Error : Cannot communicate with the device ! Option Bytes are Disabled on the device

Check the ICC cable connection and check all the needed pin connections on the ICP connector

Clock is 'External source' in this ICP mode

On Application, connect OSC pin from ICP connector or an Oscillator or a logic clock

Have tried to program other ST7 devices without any problems (ST72F561J6 and ST7MTC2J7).

jatin
Visitor II
Aug 9, 2005 4:11 AM UTC
Posted on August 09, 2005 at 06:11

As per the error message appearing, option bytes has been disabled. It means clock will be provided by the tool for the programming. So make sure the connection between Pin9 of the ICC connector and OSC1 pin of the micro is correct.

fd_it
fd_itAuthor
Associate II
Aug 9, 2005 8:40 AM UTC
Posted on August 09, 2005 at 10:40

OSC 1 is connected to the ICC connector. And i have tried to connect OSC2 to ground. Stil same problem.

The ICC connector is connected as show in the application note (ST7 FLASH STICK User Manual), see attached image.

________________

Attachments :

Image2.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I09u&d=%2Fa%2F0X0000000bUz%2FjPGn_nlvOrW91Sga8bdIgvR8i.uq8vYQCliJEtfIiZ8&asPdf=false