Skip to main content
shermantec
Associate III
Jul 10, 2003 5:20 AM UTC
Question

Problems with Emulator

Posted on July 10, 2003 at 07:20

Problems with Emulator

This topic has been closed for replies.

2 replies

romain2399
Associate II
May 17, 2011 9:34 AM UTC
Posted on May 17, 2011 at 11:34

This error occurs when:

- the emulator probe is connected to an application board not power on, or

- the ST9 of the emulator probe, the ''emuchip'', is out of order. This can be caused by an emulator power off while the application board is power on.

shermantec
Associate III
May 17, 2011 9:34 AM UTC
Posted on May 17, 2011 at 11:34

I have e problem with ST9 emulator .I allwase get ''Connection error

(LPT1) st9+cannot enter monitor mode'' when I enter debug mode.I had this

problem befor but than when I reset the software and the emulator it start

workingcorrectly .Now It alwase stays with the same error after reseting

software and emulator.

Information about leds in the emulator:

After power is on all first three leds are on (Power,Emulator reset,ST9

reset).

After start debug mode , Emulator reset led turn off and after few seconds

'St9 reset' led turn off and Run led turn on and then I got the error.

why run led turn on ??

Please answare urgently

Regards