Skip to main content
stephane2
Associate II
Aug 5, 2004 12:03 PM UTC
Question

Problem with XRAM2 mapping

Posted on August 05, 2004 at 14:03

Problem with XRAM2 mapping

This topic has been closed for replies.

3 replies

stephane2
stephane2Author
Associate II
Jul 30, 2004 11:21 AM UTC
Posted on July 30, 2004 at 13:21

Hello,

We are currently using a ST10 269 and began porting/adapting SW

to a 272b.

We are using Tasking 8 with Hitex Emulator 4.

Actually we have a start.asm file with XRAM2 declared in D0000 inside the external RAM of 256k ( A0000 - DFFFF).

In that case the XRAM2 is accessible.

But XRAM2 is not our external RAM

and should be outside the external RAM range

(e.g. 90000 with XEMU0=B930 and XADDRS3=9006) which doesn't work, What is the reason ?

Here is our configuration and part of the start.asm file :

In tasking, 2 RAM ranges are defined : 16K in D0000 and 128K in B0000

MOV R7,0x040D

MOV XPERCON, R7

BFLDL SYSCON, 0xFF, 0x0414&0xFF

BFLDH SYSCON, 0xFF, (0x0414>>

&0xFF

MOV R7,0xBD30 ; 16K XRAM2 in D0000

MOV XEMU0,R7

MOV ADDRSEL1, 0x1A06 ; External range : 256K from A0000

.....

MOV R7,0xD006

MOV XADRS3, R7 ; 16K XRAM2 in D0000

@IF( ( 0x040D & 0x07D3 ) * ( 0x0414 & 0x0004 ) )

@_MOVE ( XPEREMU, 0x040D, R0 ) ; initialize XPEREMU

@ENDI

Thanks in advance,

Stephane.

najoua
Associate
Aug 3, 2004 4:52 AM UTC
Posted on August 03, 2004 at 06:52

Hello,

I think this is due to the emulator. According to the maneer used by the emulator supplier to implement functions, you should configure the emulator using a special menu to remap XRAM2 and not by writing in XADRS3 register.

The emulator doesn't use the ST10 XRAM but a RAM memory which replaces it. Only ST10 peripherals and CPU are used. So, you should verify with the emulator supplier how to configure it.

I hope this will help you.

Najoua
stephane2
stephane2Author
Associate II
Aug 5, 2004 12:03 PM UTC
Posted on August 05, 2004 at 14:03

Hi,

We try to write in XADRS3 before enabling XRAM2 in SYSCON and XPERCON registers but it doesn't change anything.

We try now to have information from our emulator supplier.

Thank you very much for your help.

Stephane