Skip to main content
adib
Associate III
May 13, 2004
Question

Problem with STVD7 2.5.3

  • May 13, 2004
  • 4 replies
  • 1011 views
Posted on May 13, 2004 at 08:15

Problem with STVD7 2.5.3

This topic has been closed for replies.

4 replies

adib
adibAuthor
Associate III
May 5, 2004
Posted on May 05, 2004 at 08:54

Hi,

When debugging my application and placing a breakpoint somewhere in the code, the application stops and everythning is ok. If I remove this breakpoint or add a new one and then continue (F5 button) to run the application it doesn't resume (in the left down corner it shows ''Runing'').

I have to restart the application using the (Ctrl+F5) button.

Any Ideas??

alain2399
Visitor II
May 10, 2004
Posted on May 10, 2004 at 13:21

Hi,

Can you tell which micro, which version of the toolset and which debuging target you are using ?

Without those information we can't help you.

Regards
adib
adibAuthor
Associate III
May 13, 2004
Posted on May 13, 2004 at 06:09

Hi,

I am using ST72F264G2 on the IDB-ST72F264 evaluation board I wirte in ASM.

I would like to add that my software is runing on external interrupt and does almost nothing in idle.

nciot
Visitor II
May 13, 2004
Posted on May 13, 2004 at 08:15

Hi Gilat,

the problem happens because, after have reached a breakpoint and have modified it, the program runs in step-mode. Therefore you are no more in real-time mode.

I suggest you to not change/add breakpoints after the code has reached it, this will mantain the real-time condition. For more information read page 7 of the inDART-STX for ST7 User's Manual Addendum, provided with the inDART-STX installation package.

Regards,

Nicola

[ This message was edited by: Nicola on 13-05-2004 11:47 ]