Skip to main content
mailtoarup
Associate III
September 17, 2003
Question

problem with RTC

  • September 17, 2003
  • 4 replies
  • 701 views
Posted on September 17, 2003 at 04:19

problem with RTC

This topic has been closed for replies.

4 replies

mailtoarup
Associate III
September 11, 2003
Posted on September 11, 2003 at 03:35

Hello sir,

I was working with Indart demo board using Indart-St72F264 ICD……..

I have populated two Ics( M24C08 & DS1307)….on the bread board area provided in the demo board…..

And when I was communicating EEPROM(24c0

with St72F264 thro i2c communication ,then there was no problem .But when I am using RTC(DS1307-dallas semiconductor) and going thro Indart-St7 dubugger then program was not running…and was showing COMMUNICATION error………I did not use battery with the rtc. .Infact crystal was not running to its actual frequency(768KHz) .

My circuit arrangement is like that….******************************************

The micro is 32 pin ic.

I have connected pin no 5 & 6 of DS1307 to pin PA6 & PA4 of the micro respectively.

Now connection for DS1307 ::

Between pin no 1 & 2 (DS1307) connected the crystal (768 KHz)…..

A capacitor (22 pF) is connected between pin 1 & GND .Another capacitor (22 pF) is connected

Between pin no 2 & GND.

Between pin no 4 & 8 connected a capacitor(100 nF).and pin no 4 is connected to GND.

Pin no 8 is connected to Vcc(supply: 5 V D.C).pin no 8 is also connected to anode of diode(IN4007).cathode is connected to a resistance of (1K).other end of the resistance is connected to

Pin no 3.

Pin no 7 is connected to reset pin Micro thro’ a zero ohm resistor.

Actually pin no 3 is connected to GND thro’ battery(I have ommited this connection as I don’t need battery back up at his moment , this could be a problem??)

Please tell me is this arrangement is ok…….what is the cause of this problem???

pls help me in rectyfying this problem…..

Thanks & Regards

Arup

sjo
Associate III
September 11, 2003
Posted on September 11, 2003 at 06:51

I would guess the problem is pin 7 of the DS1307, as you say it is connected to the micro reset pin - why ? - disconnect this pin as it is probably reseting the micro.

I would also leave pin 3 disconnected is you have no battery, the device will only use the battery when the main power is lost anyway.

I have not used this device, but have used the very similar MK41T56

Hope this is of help

Regards

sjo
itsmejatinus
Associate III
September 12, 2003
Posted on September 12, 2003 at 14:40

Can you provide the data sheet for the RTC?

mailtoarup
Associate III
September 17, 2003
Posted on September 17, 2003 at 04:19

hi ranjeet,

i m attaching DS1.

tell me wht steps to follow to interface rtc with micro in assembly language..

i mean wht registers should be initialized..and how...

pls help

thanks

arup

________________

Attachments :

DS1307.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0CJ&d=%2Fa%2F0X0000000bV8%2FDTWe1HKrMZ.mkIRaFXdovvhNJFzXO2Q4vyAU4ftJT2U&asPdf=false