Skip to main content
jordi23
Associate II
Apr 28, 2009 2:02 AM UTC
Question

Problem with Rlink and PSDsoft

Posted on April 28, 2009 at 04:02

Problem with Rlink and PSDsoft

This topic has been closed for replies.

1 reply

jordi23
jordi23Author
Associate II
May 17, 2011 9:52 AM UTC
Posted on May 17, 2011 at 11:52

I bought the RLINK.

I have some problem program my PSD834F2.

I have in the same board one MAX7000S of Altera and one PSD834F2 of PSD - ST Microelectronics. They share the same 4-wire JTAG port ( TDI,TDO,TCK,TMS).

With the PSDsoft the Rlink Connect Test was Ok, the Target Connect Test was ok. But I have this error when I try to program PSD:

PSD JTAG-ISP Operations

PSDsoft Express 8.61 Copyright (C) 1993-2005 STMicroelectronics, Inc. All Rights Reserved.

DATE : 04/27/2009 TIME : 18:56:59

Device 1 : ( 4 pins )

ERROR: Communication (0303)

Hint: Unable to read device ID for checking.

Please check that the device is correctly connected through the JTAG port.

Time elapsed : 1 sec.

I have my Altera in ByPass...

What am I doing wrong?

I have the latest version of PSDsoft. Do I have to update the software RLINK? Jungo 01/04/2004 6.2.0.0.

Help Please.