Skip to main content
christophe239955
Associate III
Jan 24, 2006 5:23 AM UTC
Question

problem with port1.13 : HDLC

Posted on January 24, 2006 at 06:23

problem with port1.13 : HDLC

This topic has been closed for replies.

2 replies

christophe239955
Associate III
Jan 19, 2006 10:24 AM UTC
Posted on January 19, 2006 at 11:24

we want to use the HCLK for the HDLC clock (FM0 in asynchronous with DPLL for Rx) :

we are configuring one timer in output alternate PUSH PULL

GPIO_Config(GPIO0,0x2000,GPIO_AF_PP);

RCCU_PCLK(RCCU_RCLK_4);

TIM_Init(TIM2);........

TIM_ClockSourceConfig(...);

TIM_PrescalerConfig(...);

TIM_PWMOModeConfig...

+ we configure the receiver and the Xmit to use the PLL2 with the RCCU_PLL2Config(RCCU_PLL2_Mul_16,RCCU_Div_1);

HDLC_XmitClockSourceConfig(HDLC_HTXCKSource);

HDLC_XmitBaudrateConfig(7);

HDLC_RecvClockSourceConfig(HDLC_HRXCK);

HDLC_RecvClockPrescalerConfig(0);

But without doing the connection between port1.13 and port of the timer 0, we have a signal which is going out from P1.13 : which must be in????????????????????????

Thanks for explaining why we have a signal on this input 1.13?

Is it possible to use the HCLK in FMO with DPLL?

davidbellegarde9
Visitor II
Jan 24, 2006 5:23 AM UTC
Posted on January 24, 2006 at 06:23

This signal which appears on the P1.13 pin is a perturbation (about 100mV and same frequency as the HRXD) made by the HRXD pin. With the FM0 coding, no data to transmit creates 2 edges by bit. And this signal perturbs the nearest pin which is P1.13.

You could check this with the NRZI coding, the perturbation will occur only when there will be a transmission.

To avoid this, either you put P1.13 as a GPIO_AF_PP or you could shroud the HRXD line.