Skip to main content
lum
Associate II
Mar 15, 2006 7:54 AM UTC
Question

problem with GPIO internal Pull up

Posted on March 15, 2006 at 08:54

problem with GPIO internal Pull up

This topic has been closed for replies.

3 replies

lum
lumAuthor
Associate II
Mar 14, 2006 5:38 AM UTC
Posted on March 14, 2006 at 06:38

Hi,

I can't set the P0.10 gpio pull up internal resistor.

I'm using the STR710 library and the following code:

//set the P0.10 in pull up/ pull down weak input mode

GPIO_CONFIG(GPIO0, 0x0400, GPIO_IPUPD_WP);

//Set the pull up resistor

GPIO_BITWRITE(GPIO0, 10, 1);

NB : I'm using a raisonance evaluation card with a str712f microcontrollers.

Thanks.

donald
Associate III
Mar 15, 2006 7:46 AM UTC
Posted on March 15, 2006 at 08:46

P0.8 and P0.10 are ''true'' open drain rather than being push pull.

I put the question to ST about P0.8 and they indicated that the week pull up is NOT available on this pin (as part of it's 5V tolerance I believe).

The doco does not advise that weak pull up is not available.

Even after you move it to another pin be careful. If you use the library, when you change a different output pin on the same port you can change your pull ups to pull downs. This is because they do a read modify write on the port data register. When it is read it reads the INPUT state and when you write it back it sets the pull down polarity.

lum
lumAuthor
Associate II
Mar 15, 2006 7:54 AM UTC
Posted on March 15, 2006 at 08:54

thanks a lot for these informations.