Skip to main content
fabian239955_st
Associate II
Apr 19, 2006 8:47 AM UTC
Question

problem with FLASH_WordWrite

Posted on April 19, 2006 at 10:47

problem with FLASH_WordWrite

This topic has been closed for replies.

2 replies

fabian239955_st
Associate II
Apr 12, 2006 1:32 PM UTC
Posted on April 12, 2006 at 15:32

Hello,

this is an IAP with download via USB. It works fine, when I debug it, but when it runs normally, it seems to be disturbed by an IRQ, because the LR-Register is overwritten. The consequence is that it branches to nirvana. It seems to occure in FLASH_WordWrite().

Best regards,

Moe

________________

Attachments :

FW_L000100_WaMa_Download.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtNI&d=%2Fa%2F0X0000000aP8%2FB.Kier2abUDlvnsY0fWku5HjnJaJi8c8jFmxdElXbTA&asPdf=false
fabian239955_st
Associate II
Apr 18, 2006 4:56 AM UTC
Posted on April 18, 2006 at 06:56

Hi,

the frequency shouldn't be the problem. It's set to 8MHz. I don't read from flash, while I'm writing it. I use remapping to copy the flash program to the ram, to run the program from the ram.

Thanks,

Moe

[ This message was edited by: Moe on 18-04-2006 11:39 ]