Skip to main content
julien239955_stm1
Associate II
Sep 14, 2005 6:06 AM UTC
Question

Problem on USB mouse example with EWARM 430A (Error[e46])

Posted on September 14, 2005 at 08:06

Problem on USB mouse example with EWARM 430A (Error[e46])

This topic has been closed for replies.

6 replies

julien239955_stm1
Associate II
Sep 9, 2005 10:04 AM UTC
Posted on September 09, 2005 at 12:04

Hi,

I am trying to compile and execute for a STR710 the source code of the usb example provided by IAR, so it should be working straight away.

I have a problem when I link the project, I get the error

Error[e46]: Undefined external ''??divu32_a'' referred in rccu ( C:\USB_demo\Debug_Mouse\rccu.r79 )

I know that the linker had a bug, so I updated it, I have the latest version (4.59O).

Is it another linker bug?

Does anyone have the same issue?

Thanks

[ This message was edited by: ruliano on 09-09-2005 16:33 ]

julien239955_stm1
Associate II
Sep 12, 2005 9:05 AM UTC
Posted on September 12, 2005 at 11:05

OK, now I've found why it didn't work,

I had to add the file dlt4painl8n.r79 in my project under WinIdea so the compiler knows it is part of the project...

It was a problem with a div on 32 bits.

So now I can make the project, but it still doesn't work when I load it on the eval board...

Anyone has a working usb mouse project under WinIdea with IAR EWARM 430A as compiler?

Thanks

Julien

julien239955_stm1
Associate II
Sep 12, 2005 10:06 AM UTC
Posted on September 12, 2005 at 12:06

I use eval board MB 393-2.04 with the probe IONE115 (rev3) from ISystem

[ This message was edited by: ruliano on 12-09-2005 17:16 ]

nopti_albe
Associate II
Sep 13, 2005 9:13 AM UTC
Posted on September 13, 2005 at 11:13

take care that you put the right value in rccu.h

// Main Oscillator Frequency value = 4 Mhz

#define RCCU_Main_Osc 16000000

Apart from that there is nothing you can do... it should just work. On my MB393-2.04 I had to put another usb conector because the EMI-removal circuit didn't work(it took both D- and D+ high). But maybe you are lucky and don't need to do that.

julien239955_stm1
Associate II
Sep 14, 2005 5:50 AM UTC
Posted on September 14, 2005 at 07:50

Hi,

The osc value is good.

Now I'm stuck with the usb part, I receive the message

''STR71x HID Mouse demo''

on the UART, but then the program stay stuck in the routine MOUSE_init() on the loop while (pInfo->Current_Configuration == 0) NOP_Process();

I don't have any IT coming up on the USB when I plug the cable...

Plus in the Frame Number Register, D+ and D- are both set to 1 at the same time when nothing is plugged...

Hope it isn't the connector as Tudor said.

Thanks

Julien

[ This message was edited by: ruliano on 14-09-2005 11:20 ]

pchignon
Associate III
Sep 14, 2005 6:06 AM UTC
Posted on September 14, 2005 at 08:06

Hi, Julien

You remember me that you should try to download a already compiled project for the eval board.

I am asking moderator a binary file of a recognised format by winIDEA

Thanks,

Ludo