Skip to main content
sankarhari2001
Associate
Oct 20, 2004 12:48 PM UTC
Question

Problem in Programming uPSD3254A

Posted on October 20, 2004 at 14:48

Problem in Programming uPSD3254A

This topic has been closed for replies.

2 replies

sankarhari2001
Associate
May 17, 2011 10:03 AM UTC
Posted on May 17, 2011 at 12:03

Hi,

I am using RLink cable for programming uPSD3254A with PSDsoft Express. When I installed RLink driver, the PSDsoft Express provides me only one option while programming (Full chip program) and all other options (flash only...) are disabled. So I am doing a full chip programming each time. Is there any way to program only the flash. Its urgent can anybody suggest me a method to program only the flash.
joseph2399
Associate II
May 17, 2011 10:03 AM UTC
Posted on May 17, 2011 at 12:03

You can use the Ride software to program the uPSD32xx family of products. There is a programming option for just the flash. The Ride software is on the CD that was in the box with RLINK-ST. AN48 (also on the CD) explains how to program a uPSD32xx device. If you have further quesitons, please contact the applications engineering department at:

mailto:apps.psd@st.com

.

Also, in order to better serve you, please provide the following information:

Name

Company Name

Phone Number

Location (City, State, Country)

Production PSD/uPSD part number (81x, 91x, 32xx, 33xx, etc.)

Microcontroller/Microprocessor

Application

Projected annual volume (units)

Production start date

PSDsoft Express version