Skip to main content
HPARK.1
Associate II
June 17, 2020
Question

Problem CAN_ReceiveAll in standard peripheral library

I develop stm8 using cosmic compiler and v.2.3.1 standard libary.

I think there is a problem with the definition of CAN_ReceiveAll.

In this function I can get an address of _Data variable.

But, I can not get the address in Caller side.

My thoughts should be defined as:

---Caller Side---

uint8_t *pData;

CAN_ReceiveAll(&id, &pData);

--CAN_ReceiveAll Definition-- (Bold is modified)

void CAN_ReceiveAll(uint32_t* pid, uint8_t** pdata)

{

 CAN_Page_TypeDef can_page = CAN_GetSelectedPage();

 uint32_t temp1 = 0, temp2 = 0, temp3 = 0;

  

 /* select Fifo page*/

 CAN->PSR = CAN_Page_RxFifo;

  

 /* Get the Id */

 _IDE = (uint8_t)(CAN->Page.RxFIFO.MIDR1 & CAN_Id_Extended);

 if (_IDE != CAN_Id_Standard)

 {

  temp1 = ((uint32_t)((uint32_t)CAN->Page.RxFIFO.MIDR3) << 8);

  temp2 = ((uint32_t)((uint32_t)CAN->Page.RxFIFO.MIDR2) << 16);  

  temp3 = ((uint32_t)((uint32_t)CAN->Page.RxFIFO.MIDR1 & 0x1F) << 24);

   

  *pid = (uint32_t)CAN_EXTID_SIZE & ((CAN->Page.RxFIFO.MIDR4) | temp1 | temp2 | temp3 );

 }

 else

 {

  temp1 = (uint16_t)((uint16_t)((uint16_t)((uint16_t)CAN->Page.RxFIFO.MIDR1 & 0x1F) << 6));

  temp2 = (uint16_t)((uint16_t)((uint16_t)CAN->Page.RxFIFO.MIDR2 >> 2)&0x3F);

   

  *pid = (uint16_t)CAN_STDID_SIZE & (temp1 | temp2 );

 }

  

 _RTR = (uint8_t)((uint8_t)0x20 & CAN->Page.RxFIFO.MIDR1);

  

 /* Get the DLC */

 _DLC = (uint8_t)(CAN->Page.RxFIFO.MDLCR & (uint8_t)0x0F);

  

 /* Get the FMI */

 _FMI = CAN->Page.RxFIFO.MFMI;

  

 /* Get the data field */

 _Data[0] = CAN->Page.RxFIFO.MDAR1;

 _Data[1] = CAN->Page.RxFIFO.MDAR2;

 _Data[2] = CAN->Page.RxFIFO.MDAR3;

 _Data[3] = CAN->Page.RxFIFO.MDAR4;

 _Data[4] = CAN->Page.RxFIFO.MDAR5;

 _Data[5] = CAN->Page.RxFIFO.MDAR6;

 _Data[6] = CAN->Page.RxFIFO.MDAR7;

 _Data[7] = CAN->Page.RxFIFO.MDAR8;

 *pdata = _Data;

  

 /* Release the FIFO */

 CAN_FIFORelease();

 /*Restore Last Page*/

 CAN_SelectPage(can_page);

}

If I am using the API incorrectly, please advise.

    This topic has been closed for replies.