Skip to main content
d_steffen
Associate II
Jan 26, 2007 1:04 PM UTC
Question

PQFBC enable question

Posted on January 26, 2007 at 14:04

PQFBC enable question

This topic has been closed for replies.

2 replies

d_steffen
d_steffenAuthor
Associate II
May 17, 2011 7:35 AM UTC
Posted on May 17, 2011 at 09:35

Hello at all,

I use Keil MDK 3.04 in 2 target configurations:

1. Download to FLASH

Code : 0x0000000-0x0088000 512 KByte FLASH

Data : 0x4000000-0x4018000 96 KByte SRAM

2. Download to RAM

Code : 0x0000000-0x0000400 1 KByte FLASH

Code : 0x4000000-0x0010000 64 KByte SRAM

Data : 0x4010000-0x4018000 32 KByte SRAM

The first configuration is for the destination target,

but if I use it for debugging, I can only have 2

hardware breakpoints.

The second configuration is only for debugging with so many

breakpoints I want. The first code page in FLASH is needed

for the reset and interrupt vectors and some initialisation

code required from the code in the Keil Str9x.s startup file.

Now my question :

In the Keil Str9x.s startup file I can enable/disable the PQFBC

feature of the STR912 micro.

In my first configuration (Download to Flash) everything is fine,

and working, PQFBC enabled or disabled.

In my second configuration (Download to RAM) only disabled PFQBC

is working, enabling the PQFBC crashed the application.

After some checks, I rich the size of the first area,

Code : 0x0000000-0x006000 xx KBytes FLASH), with the

result, that my timer interrupt function are running not more

in SRAM and now running in FLASH, the application don't

crashed any more.

Can someone explain me this behavour, and how can I use the

PQFBC feature running completely in RAM.

Best regards

D.

d_steffen
d_steffenAuthor
Associate II
May 17, 2011 7:35 AM UTC
Posted on May 17, 2011 at 09:35

Hello Zouh,

this is not possible,

its a company project.

Best regards.

[ This message was edited by: Barricade on 26-01-2007 18:35 ]