Skip to main content
SJack.1
Visitor II
April 29, 2020
Question

Power Draw with ADC on STM8L152C6

I'm attempting to program this chip to act as a thermometer that can run on a low power solar panel. The issue I'm having is the power draw is way too high. Halted i have the power draw with an LCD and RTC interrupt ready at 5.5uA, but when I'm using the ADC the draw is over 1600uA. How can i get this draw lower?

initialization

void ADC_Icc_Init(void)

{

 CLK_PeripheralClockConfig(CLK_Peripheral_ADC1, ENABLE); //Enable ADC clock

 ADC_DeInit(ADC1); //de-initialize ADC

ADC_Init(ADC1, ADC_ConversionMode_Single,ADC_Resolution_12Bit, ADC_Prescaler_1);

 ADC_SamplingTimeConfig(ADC1, ADC_Group_FastChannels, ADC_SamplingTime_4Cycles);

 ADC_SchmittTriggerConfig(ADC1, ADC_Channel_24, DISABLE); // disable SchmittTrigger for ADC_Channel_4, to save power

ADC_DMACmd(ADC1, DISABLE);

ADC_TempSensorCmd(DISABLE);

ADC_VrefintCmd(DISABLE);

ADC_ChannelCmd(ADC1, ADC_Channel_24, ENABLE);

}

segment of main code:

GPIO_HIGH(Power_Port, Power_Pin); //turns on probe

ADC_Cmd(ADC1, ENABLE); //turns on adc

for(i=cycles; i>0; i--)

{

//Gathers Samples 

ADC_SoftwareStartConv(ADC1);

// Gathers Samples 

while( ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == 0 );

// Starts/adds to running summation of analog signal 

res = res + ADC_GetConversionValue(ADC1);

}

ADC_Cmd(ADC1, DISABLE); //turns off adc

GPIO_LOW(Power_Port, Power_Pin); //turns off probe

  // Averages Analog signal running sum //

res = res / cycles;

    This topic has been closed for replies.