Skip to main content
Reha
Associate
December 12, 2022
Question

Power dissipation of SMBJ30A/CA for DC operation below clamping voltage

Hi ST Team,

i use the SMBJ30A/CA but how much current will be flow if a DC voltage of 40 volt is applied? It must be larger than IBR = 1 mA given in the datasheet. However, there isn't any info for DC operation if a DC voltage above VBR but below VCL is constant applied.  Without this info it is not possible to calculate the power dissipation in the whole path.

Thanks

This topic has been closed for replies.