Skip to main content
mailtoarup
Associate III
December 11, 2003
Question

Pocket Flash Device

  • December 11, 2003
  • 5 replies
  • 885 views
Posted on December 11, 2003 at 02:49

Pocket Flash Device

This topic has been closed for replies.

5 replies

mailtoarup
Associate III
December 10, 2003
Posted on December 10, 2003 at 04:09

hello,

i got a pocket flash device from ST MicroElectronics from seminar which was attended by one of my friend,which contains seminar material.Now to see the contents i have to connect it to USB port and for running it i have to download some sriver software for this.Pls tell me exactly where can i find the driver and how to down load it .and how to see the content..as i have never use such device...

pls tell me in detail...all the file needed to opening up the content...

thanks,

arup

alain2399
Visitor II
December 10, 2003
Posted on December 10, 2003 at 05:41

You need a driver only under Windows 98. Under Win 2000 and XP they are provided by Windows and it works automatically, i.e Windows explorer detects and mount the PFD and a remmovable drive.

jatin
Visitor II
December 10, 2003
Posted on December 10, 2003 at 07:22

Just connect it to the USB port and use it.

mailtoarup
Associate III
December 11, 2003
Posted on December 11, 2003 at 01:24

hai,

i m using windows 98.Now tell me if i connect that memory device to

USB port then without loading any driver will this work.

i just want to be sure for safety purpose as i have no idea of using such type of device.

thanks,

arup

jatin
Visitor II
December 11, 2003
Posted on December 11, 2003 at 02:49

Yes, if you are using Windows98 then you will have to install the driver. Download ''Windows 98/ME driver Installer package'' available on the same site.