Skip to main content
daniel7
Associate II
Oct 12, 2008 9:17 AM UTC
Question

PLL frequency problem

Posted on October 12, 2008 at 11:17

PLL frequency problem

This topic has been closed for replies.

3 replies

daniel7
daniel7Author
Associate II
Oct 1, 2008 9:18 AM UTC
Posted on October 01, 2008 at 11:18

Hi.

I’m working on the STR750 eval board for a new project, and have some trouble with the PLL. It doesn’t seem like the clock changes from 4 MHz when I multiply the clock.

The interrupt should toggle a LED about 7.5Hz but instead the frequency is 0.5 Hz.If I change CKSYS to 4 MHz instead of 15x4Mhz the frequency doesn’t change.

My configuration:

void SystemSetup(void)

{

//MRCC system reset

MRCC_DeInit();

//Wait for OSC4M start-up

OSC4MStartUpStatus = MRCC_WaitForOSC4MStartUp();

if(OSC4MStartUpStatus == SUCCESS)

{

// Set HCLK to 60 MHz

MRCC_HCLKConfig(MRCC_CKSYS_Div1);

// Set CKTIM to 60 MHz

MRCC_CKTIMConfig(MRCC_HCLK_Div1);

// Set PCLK to 60 MHz

MRCC_PCLKConfig(MRCC_CKTIM_Div1);

// Enable Flash burst mode

CFG_FLASHBurstConfig(CFG_FLASHBurst_Enable);

// Set CKSYS to 60 MHz

MRCC_CKSYSConfig(MRCC_CKSYS_OSC4MPLL, MRCC_PLL_Mul_15);

}

//GPIO pins optimized for 5V operation

MRCC_IOVoltageRangeConfig(MRCC_IOVoltageRange_5V);

//Enable Timer 1, UART0 and GPIO Clocks

MRCC_PeripheralClockConfig(MRCC_Peripheral_TIM0 | MRCC_Peripheral_UART0 | MRCC_Peripheral_GPIO, ENABLE);

}

And my timer setup:

void initTimer(void)

{

/* TIM Configuration in Output Compare Timing Mode ---------------------------*/

/* CK_TIM = 60 MHz, Prescaler = 4093, TIM0_CLK = CK_TIM/(Prescaler + 1) = 656 KHz */

/* Period = 19 TIM0 Update event frequency = TIM0_CLK/ (TIM_Period+1) = 7.5 Hz */

TIM_InitStructure.TIM_Mode = TIM_Mode_OCTiming;

TIM_InitStructure.TIM_Prescaler = 4093;

TIM_InitStructure.TIM_ClockSource = TIM_ClockSource_Internal;

TIM_InitStructure.TIM_CounterMode = TIM_CounterMode_Down;

TIM_InitStructure.TIM_Channel = TIM_Channel_1;

TIM_InitStructure.TIM_Period = 1953;

TIM_Init(TIM0, &TIM_InitStructure);

/* Clear TIM0 flags */

TIM_ClearFlag(TIM0, TIM_FLAG_OC1| TIM_FLAG_OC2| TIM_FLAG_Update);

/* Enable TIM0 Update interrupt */

TIM_ITConfig(TIM0, TIM_IT_Update, ENABLE);

/* Enable TIM0 counter */

TIM_Cmd(TIM0, ENABLE);

}

________________

Attachments :

TIM.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtO9&d=%2Fa%2F0X0000000aPJ%2FaIhFvgrZscz8wNEVnmiSt4Hc.D8V16BhZPx9lo1WW_M&asPdf=false
christophe239955_st
Visitor II
Oct 2, 2008 8:24 AM UTC
Posted on October 02, 2008 at 10:24

Hi,

The maximum PCLK is 30MHz but in your configuration it is set to 60MHz.

Modify the PCLK to 30MHz : MRCC_PCLKConfig(MRCC_CKTIM_Div2);

You can also output the HCLK clock on MCO pin (P0.01 pin) to check the frequency value.

Chris

daniel7
daniel7Author
Associate II
Oct 12, 2008 9:17 AM UTC
Posted on October 12, 2008 at 11:17

I have tried to change the PCLK clock but without result.

In the testprogram I have tried to remove the MRCC_CKSYSConfig line, and the CKTIM frequency is still the same. Can the PLL be broken on the board?