Skip to main content
Visitor II
August 21, 2025
Solved

PLC module with ADC and mcu

Could you please suggest a PLC module that includes a signal scaling unit and an isolation circuit, equipped with a high-speed sampling ADC with up to 16-bit resolution? The module should also integrate a microcontroller featuring SPI, LAN (Ethernet), SD card storage, and an HDMI port.”

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
August 21, 2025

Welcome @rakesh1184, to the community!

What do you mean by PLC – Power Line Communication or a Programmable Logic Controller?

In both cases, however, STMicroelectronics does not offer ready-made modules. For these, you will need to contact the relevant manufacturers.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
August 21, 2025

Welcome @rakesh1184, to the community!

What do you mean by PLC – Power Line Communication or a Programmable Logic Controller?

In both cases, however, STMicroelectronics does not offer ready-made modules. For these, you will need to contact the relevant manufacturers.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.