Skip to main content
This topic has been closed for replies.

2 replies

thomasthanner9
Associate II
May 17, 2011 10:06 AM UTC
Posted on May 17, 2011 at 12:06

It depends on the kind of the other device. I never did this, but it might work.

P0 is the multiplexed A/D bus of the uPSD in 80pin packages. If you spend some hardware to demultiplex the data from the address and create a chip select from the address bus your other device can act just like a RAM or ROM. In this way you can exchange data between a uPSD and another device.

But if you think about coupling two uPSD directly using P0, I don't think this setup will work without a bunch of glue hardware.

qiaoren2002
Associate
May 17, 2011 10:06 AM UTC
Posted on May 17, 2011 at 12:06

I have a problem of uPSD3234, Can P0 port receive data from other device?