Question
Output Size in IDE (ROM & RAM Usage)
Posted on May 18, 2012 at 10:20
Hi everyone,
I can't find a solution to a very simple problem. STVD does not show the output size (ROM and RAM usage) when I compile with Cosmic Compiler (32K limited version). I tried many things and can see the output size in the generated map file. But I want to see it in the ''Build'' tab of STVD. Is there any way to see it after a successful compilation?Thanks in advance.Toolchain:
IDE: STVD v4.3.1Compiler: Cosmic STM8 32K v4.3.7Debugger: ST-Link V2+ #stvd-cosmic-compiler-stm8l