Skip to main content
giovanni239955
Associate III
Sep 2, 2003 1:03 PM UTC
Question

Oscillator Start up time

Posted on September 02, 2003 at 15:03

Oscillator Start up time

This topic has been closed for replies.

2 replies

kapil
Associate
May 17, 2011 9:34 AM UTC
Posted on May 17, 2011 at 11:34

This problem may arise due to the fact that after exiting the stop mode the internal clock frequency is reduced to 2 Mhz

giovanni239955
Associate III
May 17, 2011 9:34 AM UTC
Posted on May 17, 2011 at 11:34

I notice that, using a ST92F150, with a 4 MHz crystal, when I exit from Stop Mode the first instruction is executed after about 10 ms. This is not the same thing declared in the datasheet (max 5 ms).

Can you help me to fasten this behaviour? I need to be fast in order to acknowledge a message received from CAN bus.

Many thanks.