Skip to main content
daniel.benes
Visitor II
October 14, 2018
Question

Option bytes complementary error with manual write

Hello.

I'm trying to set Option bytes on STM8s005k6 from main code, but still I'm getting error in complementary bytes (when I try to rad out it back in STVP) and MCU hangs.

I'm using SDCC compiler with this code:

	// Set option bytes because of buzzer
	if(OPT->OPT2 != 0x80 || OPT->OPT3 != 0x08){
		FLASH->CR2 |= FLASH_CR2_OPT; //unlock option bytes for writing
 		FLASH->NCR2 &= (uint8_t)(~FLASH_NCR2_NOPT);
		while (!(FLASH->IAPSR & FLASH_IAPSR_DUL));
 
		OPT->OPT2 = 0x80; // enable LSI clock source
		OPT->NOPT2 = 0x7f;
		OPT->OPT3 = 0x08; // set PD4 as alternative buzzer output
		OPT->NOPT3 = 0xf7;
		while (!(FLASH->IAPSR & FLASH_IAPSR_EOP)); // wait for write finish
 
		FLASH->CR2 &= (uint8_t)(~FLASH_CR2_OPT);	//lock back
 		FLASH->NCR2 |= FLASH_NCR2_NOPT;
	}

If I set it through graphic STVP and read OPT2 and OPT3 registers, they have exactly these values. But from code it doesn't accept :\

Thank you for any tips.

    This topic has been closed for replies.

    2 replies

    Kumar B
    Associate III
    July 1, 2019

    ..

    Cristian Gyorgy
    Associate II
    July 7, 2019

    Hello Daniel!

    Ofcourse the MCU hangs. On line 5, in the while loop you wait for the DUL flag to be set, but you never write the unlocking keys to DUKR register.

    You need to write the 2 hardware keys in FLASH_DUKR register, than you can check if DUL flag is set - please check the Reference Manual for more details.