Skip to main content
emilmih
Associate II
May 11, 2007 5:24 PM UTC
Question

on program CAPS command - log message Device secured

Posted on May 11, 2007 at 19:24

on program CAPS command - log message Device secured

This topic has been closed for replies.

2 replies

mark9
Associate III
May 17, 2011 7:42 AM UTC
Posted on May 17, 2011 at 09:42

There are 2 other reasons why you get the

''Device is Secure. Select all regions for erase operation''

1. No power on the device

2. *slow* power up of the device. I discovered that if I apply 1.4V before 3.3V (ie ramp up my external power supply over the course of seconds), the device will not turn on at all. For this reason, we are putting in an external voltage supervisor, since the internal LVD doesn't seem to work well (I've verified that the LDV is enabled in the config bits).

The stupid CAPS program does not distinguish between a secured device and an unpowered device.

emilmih
emilmihAuthor
Associate II
May 17, 2011 7:42 AM UTC
Posted on May 17, 2011 at 09:42

Hi

When I try to program my STR912-SK with configuration using CAPS

it gives me log message

Start JTAG operation...

Device 1 : ( 4 pins )

Device is secured. Select all regions for erase operation.

Time elapsed : 1 sec.

And I don't think the config is programmed

When I erase ALL everything is OK

Regards Emil