Skip to main content
cstrahm
Associate
Jun 8, 2006 4:07 AM UTC
Question

Not using RTC

Posted on June 08, 2006 at 06:07

Not using RTC

This topic has been closed for replies.

3 replies

anis
Visitor II
May 17, 2011 7:29 AM UTC
Posted on May 17, 2011 at 09:29

Hi,

Just I would like to add that RTC clock is necessary if you want to exit from sleep mode, so if you are planning to use the sleep mode for low power consumption in your application then the RTC quartz should be connected.

Best Regards,

STARM

anis
Visitor II
May 17, 2011 7:29 AM UTC
Posted on May 17, 2011 at 09:29

Hi,

Yes, there is no problem to connect X1RTC pin to ground, and leave the X2RTC pin open.

Note that the only peripheral that needs the RTC clock to operate is the RTC itself, so if you are not using the RTC you can of course stop its clock.

Thanks,

STARM

cstrahm
cstrahmAuthor
Associate
May 17, 2011 7:29 AM UTC
Posted on May 17, 2011 at 09:29

I don't need the RTC in my app, can I just tie the X1RTC pin to gnd, and leave the X2RTC pin open? Don't want to use an crystal. Does anything inside care if the RTC is not running?