Skip to main content
rgovindappa9
Associate II
Mar 2, 2011 10:48 AM UTC
Question

Not coming out of Interrupt routine

Posted on March 02, 2011 at 11:48

I am using the following code for master and slave handling. When I send data from master to slave without using the interrupt routine below(by disabling intterupts) it works fine. BUT when I use interrupt routine it never comes out of it, please help  me correcting it

#stm8s-discovery
    This topic has been closed for replies.

    2 replies

    rgovindappa9
    Associate II
    Mar 2, 2011 10:49 AM UTC
    Posted on March 02, 2011 at 11:49

    My interrupt routine is as below:

    @far @interrupt void I2C_IRQHandler(void)  /* I2C Interrupt handler*/

    {

     //Handle I2C interrupts here

     I2C_HandleEvents();

     return;

     }

     

     

    void I2C_HandleEvents()

    {

     char tmp1, tmp2;

     

     

    #ifdef _MASTER_MODE_

     /*Need to remove repeting events*/

     /* MASTER EVENTS*/   

     

     /*MASTER TRANSMITTER, read-write byte=0*/

     /*Start bit sent from Master*/

     /* EV5: SB=1, cleared by reading SR1 register followed by writing DR register with Address */

     if(I2C_CheckEvent(I2C_EVENT_MASTER_START_SENT))

     {

      I2C_ClearFlag(I2C_FLAG_STARTDETECTION);

      I2C.DR = I2C.DR;//Dummy write

     }

     /* master address acknowledged */

     /*EV6:ADDR=1, cleared by reading SR1 register followed by reading SR3*/  

     else if(I2C_CheckEvent(I2C_EVENT_MASTER_ADDRESS_ACKED))

     {

      I2C_ClearFlag(I2C_FLAG_ADDRESSSENTMATCHED);

     }

     /*Master byte transmitted*/

     /*EV8_1: TxE=1, shift register empty, data register empty, write DR register*/

     else if(I2C_CheckEvent(I2C_EVENT_MASTER_BYTE_TRANSMITTED))

     {

      I2C.DR = I2C.DR;//Dummy write

      I2C_ClearFlag(I2C_FLAG_TRANSFERFINISHED);

     }

     /*Master byte being transmitted now*/

     /*EV8: TxE=1, shift register not empty, data register empty, cleared by writing DR register.*/

     else if(I2C_CheckEvent(I2C_EVENT_MASTER_BYTE_TRANSMITTING))

     {

      I2C.DR = I2C.DR;//Dummy write

      I2C_ClearFlag(I2C_FLAG_TRANSFERFINISHED);

     }

     /*Stop bit sent*/

     /*EV8_2: TxE=1, BTF = 1, Program STOP request. TxE and BTF are cleared by HW by stop condition*/

     else if(I2C_CheckEvent(I2C_EVENT_MASTER_BYTE_TRANSMITTED))

     {

       I2C_GenerateSTOP(ENABLE);

     }

     

     

     /*MASTER RECEIVER, read-write byte=1*/  

     /*Start bit sent from Master*/

     /* EV5: SB=1, cleared by reading SR1 register followed by WRITING DR register with Address */

     /*else if(I2C_CheckEvent(I2C_EVENT_MASTER_START_SENT))

     {

      I2C_ClearFlag(I2C_FLAG_STARTDETECTION);

      I2C.DR = I2C.DR;//Dummy write

     }*/

     /*EV6:ADDR=1, cleared by reading SR1 register followed by reading SR3*/

     /*else if(I2C_CheckEvent(I2C_EVENT_MASTER_ADDRESS_ACKED))

     {

      I2C_ClearFlag(I2C_FLAG_ADDRESSSENTMATCHED);

     } */

      else if(I2C_CheckEvent(I2C_EVENT_MASTER_BYTE_RECEIVED))

      {

      /*EV7_1: RxNE=1, cleared by reading DR register, program ACK=0 and STOP request*/

      if(I2C_GetFlagStatus(I2C_FLAG_ACKNOWLEDGEFAILURE))

      {

       //I2C_ClearFlag(I2C_FLAG_ADDRESSSENTMATCHED);

       tmp1 = I2C.DR;    

       I2C.CR2 &=~(I2C_CR2_ACK);    

       I2C_GenerateSTOP(ENABLE);

      }

      /*EV7: RxNE=1, cleared by reading DR register*/  

      else

      {

       //User different variable for read to care of compiler optimization

       tmp2 = I2C.DR;

      }

     }

     /* EV6_1: How is the single byte transfer info provided beforehand? */

     /* EV6_1: used for 1 byte reception only. Program ACK=0 and STOP=1 after clearing ADDR.*/ 

      else if(I2C_CheckEvent(I2C_EVENT_SLAVE_ACK_FAILURE))

      {

      I2C_ClearFlag(I2C_FLAG_ACKNOWLEDGEFAILURE);

      I2C.SR1 &=~(I2C_SR1_ADDR);

      I2C.CR2 &=~(I2C_CR2_ACK);    

      //I2C_GenerateSTOP(ENABLE);

      }

     /* slave detected stop command from master */

      /*else if(I2C_CheckEvent(I2C_EVENT_SLAVE_STOP_DETECTED))

      {

       }

    */ 

    #else //Slave mode

     

     

     

     

     /* SLAVE EVENTS */   

     

     /* SLAVE RECEIVER */

     /* Slave address matched with the address sent by master */

     /* EV1: ADDR =1, cleared by reading SR1 register followed by reading SR3.*/

     if(I2C_CheckEvent(I2C_EVENT_SLAVE_ADDRESS_MATCHED))

      {

        I2C_ClearFlag(I2C_FLAG_ADDRESSSENTMATCHED);

      }

     /* slave received the date byte from master */

     /*EV2: RxNE=1, cleared by reading DR register*/

      else if(I2C_CheckEvent(I2C_EVENT_SLAVE_BYTE_RECEIVED))

      {

      I2C_ClearFlag(I2C_FLAG_TRANSFERFINISHED);

      }

     /* Slave received STOP byte from master */

     /*EV4: STOPF=1, cleared by reading SR1 register followed by dummy writing CR2 register*/

      else if(I2C_CheckEvent(I2C_EVENT_SLAVE_STOP_DETECTED))

      {

      I2C_ClearFlag(I2C_FLAG_STOPDETECTION);

      }

     /*SLAVE TRANSMITTER*/

     /*Slave address matched with the address sent by master*/

     /* EV1: ADDR =1, cleared by reading SR1 register followed by reading SR3.*/

     /*if(I2C_CheckEvent(I2C_EVENT_SLAVE_ADDRESS_MATCHED))

      {

        I2C_ClearFlag(I2C_FLAG_ADDRESSSENTMATCHED);

      }*/

     /*Data transmited from slave to master*/

     /*EV3: TxE=1, cleared by writing DR; shift register not empty*/

     else if(I2C_CheckEvent(I2C_EVENT_SLAVE_BYTE_TRANSMITTED))

      {

        //I2C_ClearFlag(I2C_FLAG_TRANSFERFINISHED);

      //Dummy write

      I2C.DR = I2C.DR;

      }

     /*Acknowledge failure*/

     /*EV3-2: AF=1, AF is cleared by writing ‘0’ in AF bit of SR2 register*/

     else if(I2C_CheckEvent(I2C_EVENT_SLAVE_ACK_FAILURE))

      {

        I2C_ClearFlag(I2C_FLAG_ACKNOWLEDGEFAILURE);

      }  

     

     

    #endif

     

     return;

    }
    rgovindappa9
    Associate II
    Mar 2, 2011 10:52 AM UTC
    Posted on March 02, 2011 at 11:52

    My Main routine is:

     I2C_DeInit();

     _asm(''rim\n'');

     I2C_Cmd(ENABLE);

     I2C_ITConfig((I2C_IT_EVT |I2C_IT_BUF | I2C_IT_ERR), ENABLE);

     I2C_Init(100000, 0x48, I2C_DUTYCYCLE_2, I2C_ACK_CURR, I2C_ADDMODE_7BIT, 2); 

     while(I2C_GetFlagStatus(I2C_FLAG_BUSBUSY)); 

      I2C_GenerateSTART(ENABLE); 

     

     I2C_Send7bitAddress(0x40, I2C_DIRECTION_TX);

     I2C_SendData(0x22); 

     I2C_GenerateSTOP(ENABLE);