Skip to main content
fggnrc2
Associate III
Apr 21, 2011 6:33 AM UTC
Question

No workaround for STM8 assembler bug

Posted on April 21, 2011 at 08:33

No workaround for STM8 assembler bug

    This topic has been closed for replies.

    3 replies

    fggnrc2
    fggnrc2Author
    Associate III
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Robert,

    I thank you for your help (and patience...)!

    EtaPhi

    Nickname14202_O
    Visitor II
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Hello!

    In fact, instead of:

    LDW     ({MyVect-MyData},Y),X

    you have to write

    LDW     ({{MyVect-MyData}+{$ram1_segment_start-$ram0_segment_start}},Y),X

    ram1_segment_start and ram0_segment_start are defined in mapping.inc.

    ram1_segment_start is the start address in hexadecimal format of the segment where MyVect is defined.

    ram0_segment_start is the start address in hexadecimal format of the segment where MyData is defined.

    It is explained in the release notes (3rd workaround)

    Robert J

    Nickname14202_O
    Visitor II
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Hello,

    More generally, differences between two labels in two segments don't work if the segment start addresses are defined in another file.

    To avoid this, compute differences within the same segment and use constants to compute the difference between segment start addresses.

    For example, in this way:

    stm8/

        #include ''mapping.inc''

        segment 'ram0'

        BYTES

    ram0_start

    ram0_data    DS  $B7

    ram0_var     DS  1

        segment 'ram1'

        WORDS

    ram1_start

    ram1_data   DS  $AB6

    ram1_var    DS  1

        segment 'rom'

    main

        LDW     X,#{ram1_var-ram0_var} ; no, doesn't work

        LDW     X,#{{ram1_var-ram1_start}-{ram0_var-ram0_start}+{$ram1_segment_start-$ram0_segment_start}} ; ok       

        JRA     *

        segment 'vectit'

        dc.l {$82000000+main}                                    ; reset

        end

    where ram0_segment_start and ram1_segment_start are constants defined in mapping.inc:

        #define ram0_segment_start 0

        #define ram1_segment_start 100

    and

    where segments 'ram0' and 'ram1' are defined in mapping.asm:

        BYTES

        segment byte at ram0_segment_start-ram0_segment_end 'ram0'

        WORDS

        segment byte at ram1_segment_start-ram1_segment_end 'ram1'

    Sorry for the inconvenience.

    Robert J