Skip to main content
AVish.12
Visitor II
July 17, 2019
Question

No output on CCO pin even after CCOR is Enabled.

Dear Community Members,

I recently started my venture with STM8S Micro-controller. I bought an STM8S103F3P6 Chip. 

The very first thing i want to understand is Clock Control of the MCU.

Therefore i set the MCU to HSE 16MHz. Although I wanted to see if it really is working on 16MHz, I decided to use the controller's clock output capability.

Here's my main code:

#include <stdint.h>
#include "stm8s_system.h"
#include "delay.h"
 
#define F_CPU						16000000UL
 
#define RED_LED_PIN					4
#define GREEN_LED_PIN				6
#define BLUE_LED_PIN				5
 
#define DEBUG_PIN						3
#define CLOCK_OUTPUT_PIN		4
 
void main()
{
		PORTC_DDR|=(1<<CLOCK_OUTPUT_PIN);
		PORTC_CR1|=(1<<CLOCK_OUTPUT_PIN);
		PORTC_CR2|=(1<<CLOCK_OUTPUT_PIN);
		
		PORTC_DDR|=(1<<DEBUG_PIN);
		PORTC_CR1|=(1<<DEBUG_PIN);
		PORTC_CR2|=(1<<DEBUG_PIN);
		
		CLK_CCOR|=0x08;
		CLK_CCOR|=0x01;
		System_Clock_Init_External();
		
	
		
		PORTD_DDR|=(1<<GREEN_LED_PIN);
		PORTD_CR1|=(1<<GREEN_LED_PIN);
		PORTD_CR2|=(1<<GREEN_LED_PIN);
		
		while(1)
		{
				TOGGLE_PIN(PORTD_ODR,GREEN_LED_PIN);
				TOGGLE_PIN(PORTC_ODR,DEBUG_PIN);
				delay_ms(20);
		}
}

Here's how i am accessing registers:

#define OFFSET_ADDRESS			0x5000
#define SFR(addr)				(*(volatile unsigned char *)(OFFSET_ADDRESS + (addr)))
 
#define PORTC_ODR					SFR(0x0A)
#define PORTC_IDR					SFR(0x0B)
#define PORTC_DDR					SFR(0x0C)
#define PORTC_CR1					SFR(0x0D)
#define PORTC_CR2					SFR(0x0E)
 
#define CLK_ICKR					SFR(0xC0)
#define CLK_ECKR					SFR(0xC1)
#define CLK_CMSR					SFR(0xC3)
#define CLK_SWR						SFR(0xC4)
#define CLK_SWCR					SFR(0xC5)
#define CLK_CKDIVR				 aSFR(0xC6)
#define CLK_PCKENR1				SFR(0xC7)
#define CLK_CSSR					SFR(0xC8)
#define CLK_CCOR					SFR(0xC9)
#define CLK_PCKENR2				SFR(0xCA)
#define CLK_HSITRIMR			 SFR(0xCC)
#define CLK_SWIMCCR				SFR(0xCD)

Here's my external clock init function:

void System_Clock_Init_External(void)
{
	CLEAR_REGISTER(CLK_ICKR,0xFF);
	SET_BIT_IN_REGISTER(CLK_ECKR,0);
	while(!(READ_REGISTER_BIT(CLK_ECKR,1)));
	CLEAR_REGISTER(CLK_CKDIVR,0xFF);
	SET_REGISTER(CLK_PCKENR1,0xFF);
	SET_REGISTER(CLK_PCKENR2,0xFF);
	//CLEAR_REGISTER(CLK_CCOR,0xFF);
	CLEAR_REGISTER(CLK_HSITRIMR,0xFF);
	CLEAR_REGISTER(CLK_SWIMCCR,0xFF);
	CLEAR_REGISTER(CLK_SWCR,0xFF);
	SET_REGISTER(CLK_SWR,0xB4);
	SET_BIT_IN_REGISTER(CLK_SWCR,1);
	while((READ_REGISTER_BIT(CLK_SWCR,0)));
}

When i check the output on pin PC4 on an Oscilloscope, all i get 1.4V DC Voltage.

What is it that i am missing?

This topic has been closed for replies.

1 reply

DGoul
Visitor II
August 6, 2019

Do you mean to set HSE, or HSI. That is, do you actually have an external 16 MHz clock signal, or are you using the internal highspeed oscillator?