Skip to main content
mariusz2
Associate III
Apr 4, 2007 5:43 AM UTC
Question

new user problem str911 first start

Posted on April 04, 2007 at 07:43

new user problem str911 first start

This topic has been closed for replies.

1 reply

mariusz2
mariusz2Author
Associate III
May 17, 2011 9:31 AM UTC
Posted on May 17, 2011 at 11:31

Hi all.HI.thi is my first steps to programing in ARM. I began programming software in str911fm44. I use STX-link and raisonanse development tools. I have several problems:

1) How connect j-tag 20 pins to str911fm44 ?

I d'not find to ST sites example

2) I connect j-tag connetor via example F-link (st www sites) 14 pin connector. At present time, I can olny programing flasch memory, and run program it is OK,

in debug mode I Have message ''unable yo communicate witch target CPU''. How run i debug mode (may by jtag conetetcor is connected improper (badly)?

3) I have a problem witch initialize PPL clock mode all function returns error: (SCU_PLLCmd(DISABLE)-ERROR,SCU_PLLFactorsConfig(_PLL_N, _PLL_M, _PLL_P)-ERROR,SCU_MCLKSourceConfig(SCU_MCLK_OSC)-ERROR, without one ( SCU_PLLCmd(ENABLE))

I use library stdlib from St site

If possible plesase send me example with initialise PLL clock (I Use crystal 11,0592 Mhz)value PLL_M, PLL_P PLL_N generate caps software.

All examples from st site not run.

only function printf is ok.

while(1)

{

printf(''U'');

}

I obsere wavwform to scope uart0, node TX0, spped is not compatybile with standards uart speed, one frame about 2 ms

please help me. best regards Mariusz