Skip to main content
Associate
September 2, 2023
Question

Need help with the creation of new app. in Android Studio to communicate with STEVAL-MKSBOX1V1

Hi everyone,

I'm trying to create a new application for my Computer engineering degree. What I have to do is to create an Android application an program the board STEVAL-MKSBOX1V1 in pro mode. Now I'm doing the Android part: I've an app with 3 buttons each one with a label. I want to create a file excel in which I put the label and the data which came from accelerometer and gyroscope of the board. I had found a library on github for the BLE connection etc. and I'm trying to use it...but I have some problem because I don't understand how to use it. Is possible to have some examples or some advices?
Thank you.

 

    This topic has been closed for replies.

    2 replies

    Issamos
    Super User
    September 2, 2023

    Hello @Ila 

    I suggest you to take a look at this library. You can find a ready to use project. You have to adapt it to the application you need to do. 

    Best regards.

    II

    IlaAuthor
    Associate
    September 5, 2023

    Thank you so much.
    I need something related to Android Studio develop because I'm using it to programm the Android App. I've already done the schede part with STM32CubeIDE. Now what I have to do is write on Android Studio the application I have explained...
    The library and the documentation I've found is this: https://github.com/STMicroelectronics/STBLESensor_Android 
    And based on this I want to produce my app...
    I have only 6 days to do it and I'm afraid becuase I'm not on a good point. If is usefull I can share my code.

    Best regards.