Skip to main content
RPith.1
Associate
May 26, 2021
Question

My stm8s103f3p6 breakout board works with 5v/9v adapter supply but not with 9v battery.

The circuit works fine with 5v/9V adapter supply but when we connect with 9v Battery controller could not work as expected.

I have assembled stm8s103f3p6 break out board with my circuit, which have below gpio connections!

//Chip_Pin_No.  Pin Name   Connected with

//  5..............................A1................................. 

//  6..............................A2................................. 

//  10............................A3.............LED

//  11............................B5...............................     

//  12............................B4.........Keyboard switch 

//  13............................C3.........Keyboard switch 

//  14............................C4.........Keyboard switch 

//  15............................C5.........Keyboard switch

//  16............................C6.........Keyboard switch

//  17............................C7.........Keyboard switch

//  18............................D1.........Keyboard switch 

//  19............................D2.........BUZZER  

//  20............................D3.........SOLENOID  

//  1..............................D4.........LED  

//  2..............................D5.................................  

//  3..............................D6.......................  

For Buzzer and solenoid connections: controller pin D2/D3 >> 100 Ohm >> S8050(J3Y) transistor. (already Tried out 1k and 10k resistors instead of 100 Ohm with parallel 100nf capacitor)

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    May 26, 2021

    Have you measured the current? Does the voltage drop?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    RPith.1
    RPith.1Author
    Associate
    May 27, 2021

    yes, Observed Lower voltage at the time of triggering of buzzer from controller.

    Function is like when we press any switch buzzer sounds like the BEEP. But in case of malfunction(when connected with 9V battery) buzzer's beep is like very poor and disturbing nature.

    RPith.1
    RPith.1Author
    Associate
    May 27, 2021

    .