Skip to main content
Associate
February 19, 2025
Question

MOSFET N

Hello, I need an N-channel MOSFET that operates perfectly as a switch (on/off) with a gate voltage range of 0V to 3.3V. Could you recommend one? image-20250114-161053.png

This topic has been closed for replies.

3 replies

Peter BENSCH
ST Technical Moderator
February 20, 2025

Such PWM is usually generated with significantly more than 10Hz, for which a MOSFET is usually no longer controlled directly from the PWM output, but via a gate driver.

However, if you drive the pump from 5V, the gate driver can also use 5V, which makes it easier to select the MOSFET.

In addition, you have not specified the required current of the ‘Pompe’ (pump?).

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Javier1
Principal
February 20, 2025

Dempends of the size of your pump
but these should work (gate + mosfet inside the same dice)

Javier1_0-1740053110742.png

 

hit me up in https://www.linkedin.com/in/javiermuñoz/
AScha.3
Super User
February 20, 2025

Hi,

typical for this, i use logic level mosfets :

- (not too much current, small load) IRLML6344 , 30V , 4A ; SOT-23 ;

- (for bigger power:)  IRL540 , 100V , 30A ; To220

 

-- or any other logic level mosfet, that matches your load.

If you feel a post has answered your question, please click on " Best Answer ".