Skip to main content
julienduay
Associate III
Feb 16, 2006 6:12 AM UTC
Question

MMC or SD card in SPI mode with STR710

Posted on February 16, 2006 at 07:12

MMC or SD card in SPI mode with STR710

This topic has been closed for replies.

4 replies

julienduay
Associate III
Feb 15, 2006 4:29 AM UTC
Posted on February 15, 2006 at 05:29

Hello everybody.

Can I transfer data on a MMC or SD memory card (in SPI mode) with the BSPI interface of STR710 micro-controller?

Thank you

fa_it
Associate III
Feb 15, 2006 5:29 AM UTC
Posted on February 15, 2006 at 06:29

Yes, it is possible.

julienduay
Associate III
Feb 15, 2006 9:15 AM UTC
Posted on February 15, 2006 at 10:15

Thank you for your answer.

Did you already use SPI signals for reading and writing on a SD card?

Is there a free example on the Web for the memory card driver?

fa_it
Associate III
Feb 16, 2006 6:12 AM UTC
Posted on February 16, 2006 at 07:12

Look at

http://www.ulrichradig.de/

best regards, Frank Andersen